This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS80PCI102: Can DS80PCI102 used with PCIe Gen3 two lane application ?

Guru 19785 points
Part Number: DS80PCI102
Other Parts Discussed in Thread: DS80PCI402

Hi Team,

Customer is using DS80PCI102 for PCIe Gen3 two lane application. Can they use this device without communication problem ?

I think DS80PCI402 would be a better approach because they could use same device for the two lanes, instead of using two devices for each lane if using DS80PCI102.

I also understand that PCB design would be easier using DS80PCI402.

However, since they do not have registered the device in their company they cannot use DS80PCI402.

Could you advise us if DS80PCI102 could be used for Gen3 2/4 lane application ?

Best Regards,

Kawai