Part Number: XIO2001
Hello,
Regarding to VDD_33_AUX on XIO2001, my customer is asking some question.
(Question)
(1) When VDD_33_AUX is not used, is external pull-down needed?
(2)If so, how much resistor value is needed?
(According to 9.2.1.1.3 Auxiliary Power(D/S page115), it is greater than 3kΩ.)
Do you have recommendation resistor value?
(They will use 3kΩ. It's OK?)
Regards,
Tao2199