Part Number: TPS65982
Other Parts Discussed in Thread: , TPS65981
Hello TI Team,
I'm having a little trouble connecting a TPS65982-EVM to my PC.
Instead of using an Aardvark or FTDI connection I wanted to use the USB EP option. However, neither the "Utilities GUI" (using: Configure -> Test Configuration Setting) nor the "Application Customization Tool" seem to be able to connect to the board. Both application return the error: "ValueError: No backend available" (when trying to execute the hw_open function in the corresponding python script). Furthermore there isn't even anything visible in the Device Manager on Windows (or on /dev/ on ubuntu respectively) when connecting the EVM via the USB-C to USB-A cable to a PC, so I can't even try to talk to the board 'by hand'.
I power the EVM via Pin2 of the J5 jack (the System_5V rail) of the board (which also seems to power the System_3V3 rail). Besides the power LED, the cc1 LED (or cc2 LED) is also lighting up when the USB-C cable is connected.
Connection the EVM to a PC this way should work, shouldn't it? Or am I missing something?
regards
Tobias Eckhardt