What is the Rosenberger part number for the HSD connector talked about in the '926 eval user guide?
The BOM and the associated text does not contain the part number.
I have searched the various forum posts. I found this BOM for the '928: http://www.ti.com/lit/df/tidrwd0/tidrwd0.pdf
it says the part number is D4S20D-40ML5-Y (and) Rosenberger Automotive HSD Connector - Right Angle Plug for PCB. DO NOT PURCHASE. TI WILL PROVIDE.
Is this the right part number? Will TI provide the J1 connector? Why does one BOM for one eval kit specify this detail, and others do not (hint, hint)?
Why is the user guide not explicit in the discussion on using the HSD connector about what the part number is && TI will provide it?
Short version: why are you making it hard on the engineer? Why are you forcing us to waste our time figuring out something you should just be telling us?
(Not trying to sound harsh. TI makes good stuff, and for the most part, the documentation is good to excellent. Just frustrating when these details get dropped.)
It does make sense to use the same part for the SER & DES to keep the cabling simple. In my case, the '926 is the DES; the SER will be the '947 (both appropriate eval kits).
I note the '947 eval kit uses the D4S20D-40ML5-Z, so it makes sense the '926 eval kit should use the same connector. Be nice if it was in the BOM (hint, hint)
Since I am asking for specifics, if the same HSD connector is on both ends, what is a good part number for the cable?
(Yes, I could probably look it up on the Rosenberger website, but why not make it specific?)
speaking of hints for missing information:
Where you have a case of the SER & DES eval kits using the same connectors, PLEASE include the part numbers for the cables!
For the '913 // '914 you give the details, but I first looked at Digikey and Mouser for the cable - no joy.
I then explicitly googled the exact text and found the proper cable.
So you left enough of a breadcrumb trail, but I thrashed for a bit before I got smart. The cable part number and source should be in the BOM when possible.
And when not possible, enough information so w can make our own..
(BTW, it might just be my computer setup, but a line long enough to wrap gets really funky when it wraps
- the wrapped text is half a line height, not a full line height. this is an example.
And when the line wraps, the cursor wants to be stuck at the end on the line - it will sometimes not move if you click inside that line (say to correct a typo).
You do eat your own dogfood...??? (That is a technical term. it means you use your own product, or customer-facing system.)