Part Number: ISO3082
Hello all,
When I used ISO2083 to communicate with my computer via serial port to USB,Part of the data received by the computer was wrong.9 bytes of frame data, the first 4 are correct, and the last 5 are uncertain.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO3082
Hello all,
When I used ISO2083 to communicate with my computer via serial port to USB,Part of the data received by the computer was wrong.9 bytes of frame data, the first 4 are correct, and the last 5 are uncertain.
Hi Wade,
Two things would really help me debug this issue:
As well as those two items, does this happen every time or is the error sporadic?
Thanks for contacting us on E2E!
Best regards,
Dan
Hi Wade,
Thanks for providing a schematic. At first glance I do not see anything wrong in the schematic.
Do you have any scope shots of the data?
Have you tried any other RS-485 transceiver in the same setup and seen a different result?
Best regards,
Dan
Hello Dan,
When sending 0 continuously, the PC side receives an error. The phenomenon is the same as ADM2483 .