Part Number: TUSB8041
Dear Specialists,
My customer is considering TUSB8041I and has a question.
I would be grateful if you could advise.
---
Regarding TUSB8041I,
How is the difference of transmission ability each device.
I am thinking of using multiple devices to perform transmission of USB 3.0 full bandwidth.
I am concerned about how the individual difference in performance will affect the system.
Exact values are not necessary, it is enough to know the order.
(For example, Individual differences should be less than 0.3% when excluding clock variations, etc.)
Also, is there a relatively large variation factor besides external clock?
I think that the accuracy of the external clock is major factor of performance change, I' like to know the other.
---
I appreciate your great help in advance.
Best regards,
Shinichi