Hi,
I've got this chip on a custom board using the fiber interface and, even though I have full connectivity with other devices on the network, I've noticed that BMSR(2) bit, Link Status, isn't set to '1' when the link is in fact ready, as I can send and receive packages.
If this bit isn't set, maybe is it because while under fiber mode, another one is? How could I check for link status under these circumstances?
Thanks, best regards