Part Number: 88E1518
Hi ,
We are using 88E1518 in one of our design.
In Frist production slot of 100 Boards are assembled with Date code of 2014 and boards are working fine [When we do ping 0% packet loss ]without any issue.
in Second production slot of 50 boards are assembled with Date code of 2017 and all boards are giving inconsistent results [When we do ping , it works fine for 2-3 mins after than packet loss increased to >50%]
Please let us know is there any recommended Other setting need to be done for 2017 date Code IC's??
FYI: Driver configurations, ETHERNET PHY settings and Board manufacturer is same for First and Second slots.
Any help to resolve this issue is highly appreciated.
Thanks,
Harshavardhan.