Part Number: SN75DP159
Hi,
I'm using SN75DP159RSBT & TMDS181RGZT in a single board, so I have made the VDD voltage as 1.15V to keep the common source for the two.
As per the datasheet range, the input voltage 1.15V matches as the common voltage for the two devices.
So can anyone please confirm that this sharing of inputs and input of 1.15V on VDD correct for both the devices.
Thanks & Regards,
Nanjunda M