Part Number: TLK10232
Hi Team,
As you know , there are 2 port in TLK10232.
I know that TLK10232 is reqired cofigulation.
And I'm writing following address , data to both port.
*Disable auto-negotiation by writing 1'b0 to 0x07.0000 bit 12
*Disable link training by writing 16'h0000 to 0x01.0096
*Write 16'h03FF to 0x1E.8020
*Changing HS_ENTRACK (0x1E.0004 bit 15) to 1'b1 and HS_EQPRE (0x1E.0004 bits 14:12) to 3'b101
*clkpll cfg
*Issue a data path reset by writing 1'b1 to 0x1E.000E bit 3
I would like to confirm timing of sending reset command to TLK10232.
( Reset command: Issue a data path reset by writing 1'b1 to 0x1E.000E bit 3)
Case 1: Set A port register and then send reset command for A port . Set B port register and then send reset command for B port.
Case 2: Set A port register and set B port register and then send reset command to A port and B port.
Which is better ?
Are there any problem in initialize or data transfer?
Regards,
Yoshihiro