Part Number: DP83848I
Other Parts Discussed in Thread: DP83822I
Dear Sirs,
I'm using the DP83848I with STM32F207 in RMII mode.
It seems to be working well, but checking the timings for RXD[0:1] from the Phy, I found that the minimum delay from X1 rise to data transition is 2ns (T2.25.2 in datasheet), while the STM32F207 requires a hold time tih(RXD) on these signals at least 1.5ns. It means that there are only 500ps as max skew between the clock and RX data at the uC ports. Furthermore, due to temperature, aging, clock slpes, etc... this timing seems to be very critical. My questions are:
-what's your opinion about this?
- are you aware of any design using DP83848I and STM32F207 in RMII mode
- since the declared value for T2.25.2 is very spreaded (2ns to 14ns!!!) do you think there are conditions where it is granted a min time greater than i.e. 3ns instead 2ns (for example, in case the min temperature is -25°C instead of -40°C)
I look forward to your kind reply.
Best Regards,
Alberto.