Part Number: SN6505B
Other Parts Discussed in Thread: SN6501,
All,
I'm looking to use the SN6505B for generating a dual ±20V supply from a single +5V supply. This would be for a low load current application (probably < 5mA). There's an application shown in the SN6501 datasheet on page 21, figure 48, showing a half-wave rectifier without center tapped secondary that should work.
Is there a reason that this application is shown on the SN6501 datasheet and not on the SN6505B datasheet? It seems like the application would work for both devices.
Joseph Wu