This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB921 maximum video resolution

In this page http://www.ti.com/interface/fpd-link-serdes/display-serdes/overview.html the DS90UB921 and DS90UB922 seem to support FULL HD resolution but the max pixel clock frequency is 96MHz.

Are these device capable to manage a resolution of 1920x1080 @50/60Hz. Can you confirm that the only devices that support 1920x1080 are 947,948 and 949 ???

I'm investigating on the possibility to use the FPD link III technology to connect devices in daisy chain mode up to 18/20 meter link... The source is an HDMI that need to be displayed on local TFT then the video signal is forwarded to another display via FPD link III then displayed locally and forwarded to another display and so on.

I need also to have a back channel (SPI, I2C, UART) to control/check the "remote" display.

The needed resoultion is 1920 x 1080 60Hz.

The local TFT panel have a LVDS interface (OpenLDI)

Is the FPD link III technology supports max cable length of 18/20 meters?
There is an IC that can serialize / deserialize a 1920 x 1080 60Hz with RGB 24 bit input/output?

Thank you in advance for you answer