Part Number: ISO5452
Other Parts Discussed in Thread: TL431
Hi team,
In order to size our insulated power supply for the ISO5452 +15V/-8V application, my customer would like to estimate current levels passing through GND2.
1- Does the “IQ2 Output supply quiescent current 6 mA” flows through/to/from GND2 or rather directly from Vcc2 to Vee2?
2- Do they have other currents that passes through GND2 than the blanking capacitor ones?
- “I(CHG) Blanking capacitor charge current 0.5 mA” (assuming that the blanking capacitor is connected to GND2 as Fig 50)
- “I(DCHG) Blanking capacitor discharge current 14 mA”
Do they have to consider other currents through GND2?
Thanking you in anticipation
Pol
PS
We’ve noticed that on fig 29 of the TL1431, the bipolar type should be a PNP rather than a NPN