Part Number: TUSB422
Other Parts Discussed in Thread: AM5748, TPS65982
Tool/software: Linux
Hello
I got TUSB422_SW software from TI and I tried to compile the Linux driver wit TI Linux SDK 4.3 as suggested in TUSB422 Linux Driver Users Guide.pdf
- Copied the contents of tusb422_linux_v0.99 to ./drivers/usb/tusb422 (maybe there is a more suitable place. There is no hint in the doc)
- Added “obj-$(CONFIG_TUSB422) += tusb422/” to ./drivers/usb/makefile
- Added “source drivers/usb/tusb422/Kconfig" in ./drivers/usb/Kconfig in line 108
Kernel config:
CONFIG_TUSB422=y
CONFIG_TUSB422_PAL=y
Finding 1: It does not compile because string.h is not included if CONFIG_TUSB422 is set.
#ifndef CONFIG_TUSB422
#include <linux/string.h>
#endif
I can correct that, but I wonder if this driver was ever compiled under Linux by TI??
Finding 2: It does not compile due to missing include file in usb_pd_pal.c : #include <huawei_platform/usb/hw_pd_dev.h>
In the TUSB422 Linux Driver Users Guide.pdf there is a hint that "USB PD platform abstraction layer (PAL) must be ported to enable the software for use on specific platforms.". There is no hint how to implement these function in usb_pd_pal.c. Brian Quach from TI commented "A platform abstraction is required and an example for a Huawei platform is included". In fact, there is no such example included.
In addition to the PAL there is also a lot of parameters that can be set in the device tree, see tusb422-pd.txt. There are parent a child nodes but no explanations how to use.
I need help for our simple use case:
- Schematic as below (has been reviewed by TI). TUSB is connected to AM5748 USB port 1 or 2. We use USB type C connector and want to run USB 2.0 and 3.0.
We would like to test 2 scenarios:
Scenario 1): Ethernet over USB. This is for testing device mode.
CPU USB port is in device mode, Ethernet gadget active.
Windows PC connected with USB type A to type C cable
Scenario 2): Access to USB-C memory stick. This is for testing host mode.
---
Would it be possible to support us for these I guess quite simple scenarios?
We would need help here:
- Suggested device tree settings according to tusb422-pd.txt
- Suggested minimal implementation of platform-specific functions in usb_pd_pal., if required at all for the given scenarios (by setting CONFIG_TUSB422_PAL=n ?)
Our USB interface can deliver 5V / 3A.
Regards, Chris