Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: ALP
Hello All,
We have a custom board using the DS90UB953 serializer. We are currently having problems trying to get the the serializer to form a stable link with the DS90UB954 EVM even using the ALP software. We currently do not have the sensor connected and are just trying to get a link in synchronous clocking mode over coax. The link has a pattern of sporadic for ~200ms and then drops out for ~400ms. Also I have a few more questions below from my debug thus far.
1. Should the refclock feeding the 954 should be correlated in reconstructed CLKOUT of the Serializer? They are the same frequency and are stable but have no correlation.
2. Do we need to configure any registers to get the initial link between the 954/953?
Thanks,
Ben Roy