Part Number: TPD12S016
Other Parts Discussed in Thread: TPD12S521, TPD12S520
I am driving an HDMI source via an FPGA. I am having a problem where the required TMDS pull-up resistors in the sink (monitor) are feeding current back into my FPGA when the FPGA is power off, but the monitor remains on. This current is keeping my FPGA in a quasi-powered state.
It looks like the TPD12S016 might do what I want, but it is unclear to me if the chip will specifically prevent (provide a path for?) the current I have described above? The datasheet indicates:
"Back-drive Protection on HDMI Connector Side Ports"
But does that mean the chip protects itself and will not provide a path for back-drive current, or does that mean it protect the signal lines from back-drive current as I need?
If is does not provide the kind of protection I need, is there a TI chip that does?
Thanks,
Matthew