Part Number: TMDS181
Hi everybody!
There is a question about TMDS181 data sheet: SLASE75D.pdf.
1: When not using the SPDIF_IN function, it is described as GND and connection via 500 kΩ,
Is it mandatory? Also, could you tell me if there is a tolerance of 500 kΩ?
2: It is recommended that the resistance value of Pull-UP / Down setting each control pin is 65 kΩ, but can it be changed to 62 kΩ or 68 kΩ etc.?
(Is it ok to think that it is within the range of 65 kΩ ± 10%?)
3: It is recommend 55 Ω ARC output terminating resistor,
If not used ARC function, may it be 49.9 Ω or 51 Ω etc?
4: It is recommend VSADJ, 7.06 kΩ 1% ,
I think used 7.04 kΩ is good enough, is there a problem?
Please let me know if you have any information.
Best Regards
Shing