Part Number: DP83822I
Dear Specialists,
MY customer is evaluating DP83822I and encountering a problem.
I would be grateful if you could advise.
---
According to the datasheet, When LED_ 0 is using for BLINK for TX/RX Activity, should be use MODE1 or 2.
I choose MODE1(1.96ohm pulldown) at LED_0pin, but it output H stable instead of blinking when ethernet had established.
Related resister data is listed below.
Table 40. 0x0019 PHY Control Register (PHYCR) BIT5 LED Configuration is 0
Table 46. 0x0025 Multi-LED Control Register (MLEDCR) BIT6:3 MLED Configuration (COL Pin) is set 0000(default).
0x0019 Bit 5 is strapped pin, so it doesn't need to set the resister.
0x0025 Bit6:3 are not strapped, are these need to set the resister?
Are there any resisters to set?
Does this means it is impossible to set "BLINK with TX / RX communication" only by Strap pin connection?
---
I appreciate your great help in advance.
Best regards,
Shinichi