Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65983: charging problem between tps65983 and tps65988

Part Number: TPS65983
Other Parts Discussed in Thread: TPS65988, TPS65987D, TPS65981, TPS65982

HI,

    We designed a mini-charger based on tps65983. The charger is used to charge Lenovo's TABLET 10. Lenovo tell us the PD IC in the Tablet is tps65988.

If we set the source capabilities of tps65983 to 12V/3A, the tablet can be charged, the actual charging current  is  3.05A, but the charger and internal tps65983 is very heat.

We need to lower the current to lower the heat. So  we change  the source capabilities to 12V/2A. But the charging current is not stable, rise up to about 2A and then drop to 0 immediately, and then rise again , drop , go round and round. The tablet can not be charged , the battery's capacity does not increase.

My Question is:

Why does not the tablet limit  it's charging current to 2A  when the charger's the source capabilities is limited  to 2A?

And how to lower the tablet's charging current? By  the charger side(tps65983) or tablet side(tps65988)?

Thanks.

  • Hi Zhifeng,

    The TPS65983 is only to be used in TBT devices that are following an Intel reference design. It sounds like that is not the case here. I would recommend using the TPS65981 or TPS65987D for this application instead. The TPS65987D is capable of doing up to 5A on the internal power path.

    The table will limit its charging current to 2A when the source capabilities is 2A because the negotiated PD contract would read 12V/2A. Per the PD Spec, the table should not draw more than 2A.

    If this answers your question, PLEASE select This resolved my issue

    Thank you,

    Eric

  • thanks,Do you mean the tps65983 can not be used for charger if non TBT ? Our charger only perform charging, no usb-data or display data . We only connect the VBUS, GND , and CC1 line to the Tablet.

  • Hi Zhifeng,

    That is correct, I would recommend swapping out with the TPS65982 as it is pin to pin compatible with the TPS65983. If you want to use the TPS65987D to support 5A sourcing, you would need to adjust the layout since the package is different.

    Thank you,
    Eric
  • But i still  can not understand why you said tps65983 can not be used in charger without TBT?

    1. My charger works well  with the USB-type C PD product. The tablet is  USB type-C PD3.0.  the PD power negotiation with the tablet is OK.

    Battery charging is OK , but  very heat when the current is 3A.

    2. I bought a TPS65983EVM from TI store. It can configure to emulate many aplication  type through DIP swich. The application type include not only thunderbolt notebook,

    but also High power charger adapter, mid powr charger adapter.

    Can I use  tps65983 to design a USB type-C PD2.0 charger ?

  • Hi Zhifeng,

    Unfortunately, we are only allowed to give the configuration tool for the TPS65983 for people who are using it in Thunderbolt device designs. This is controlled by Intel. I understand that the TPS65983 works well in your application but I can only recommend the TPS65982, TPS65981, or TPS65986 for this application as it is NOT a TBT device design.

    Thank you,
    Eric
  • 1. I read the tps65982 datasheet, it also support thunderbolt, what's the difference between 982 and 983 on thunderbolt?

    2.Does the tps65983A GUI configuration tool has some templates  to configure as  charger , which is similar to TPS65982's templates, see following:

    Can you give me the corresponding snapshot of TPS65983A GUI configure template?

    Thank you.

  • Hi Zhifeng,

    The TPS65982 can be used in TBT Host Systems. The TPS65983A can only work in TBT Device systems. The TPS65983A GUI only contains templates that exactly match the intel reference designs. Also, the TPS65983A GUI has very little configuration options open to the customer as everything is already set to match the specific reference design.

    Thank you,
    Eric