Part Number: DP83867IR
Other Parts Discussed in Thread: MIO
Tool/software: Linux
I have a question about using two ethernet PHY chip DP83867IRPAPT interface with Zynq7010 MIO PS interface. I have first PHY without Address strap so it address is by defualt 00000(b), the 2nd PHY with strap mode2 on RX_D4, so this PHY's address should be 10000(b) by design. The problem is that when running software, zynq7010 always get the address to be 01111(b) and 11111(b) respectively. It looks like the address strap does not work OR distorted. Does anybody has answer about this issue? Thanks.
Ping
P.E.