Part Number: TPS65981
Hello,
I am working with a customer who is have trouble getting data out of the TPS65981 USB 2.0 MUX.
They are able to pass the D+ signal out of the USB_RP port to their SoM, but when the D- signal is connected the signal goes to 0 V.
When the RP port is not connected to the SoM, the USB_RP pins show D+ and D- working fine.
When the TPS65981 is bypassed completely, and the USB port is connected to the SoM, the USB works fine.
Both the D+ and D- pin going to the SoM ohms out at 200Kohms w/ respect to ground, the resistance on the USB-PD measures open.
Do you have any ideas as to what could be causing this behavior?