Part Number: DS100MB203
Other Parts Discussed in Thread: TLK10034
Hello,
In the datasheet of the device, for 10GBASE KR mode selection , different values are given .
In the pin functions table, it is mentioned that the device MODE pin to be set as "1" .Whereas in the SMBUS slave mode register map, register 0x25 bit 6 value is to be set as "0" for 10GBaseKR mode. This looks conflicting.
What is the value to be set for MODE pin when in 10GBaseKR ?