Part Number: TUSB522P
Other Parts Discussed in Thread: TUSB8020B
Hello,
I am currently looking to incorporate the TUSB522P into a USB 3.1 Gen 1 transmission line with an expected high insertion loss between two TUSB8020B hubs.
1. Per answers in threads such as this one, it appears that the method to determine the right selection of EQ/DE/OS settings is to choose conservatively and work from there in the absence of concrete simulation data. In your experience, is a protocol analyzer or simulation model really needed here for the integration of this product to be effective?
2. In this forum question, a customer asked if "it a good idea to place a hub part downstream from the host in an effort to "retime" the USB channel, possibly also putting redriver parts on both sides of the hub," but it looks like there wasn't an answer given. Assuming the region contributing to the insertion loss is known and discrete, would it be preferred to have a redriver before, after, or on both sides?
3. In this forum question, it was stated that "the usage of two or more re-drivers (especially for USB3) may cause over equalization issues." Is there a method to determine when this will be the case?
Thank you for your time and best regards,
Kyle