Other Parts Discussed in Thread: DS90CF364A
Hi,
We're trying to drive a two low resolution LCD displays, 480 x 270, and the maximum pix clock frequency of the display is 10.99 MHz. The interface has to be LVDS to RGB, but the only LVDs to RGB converter I can find is the DS90CF364A. The spec. for the part has a minimum clock frequency of 20MHz, but could it still operate as 12 MHz ? if not, what are my options ?