Part Number: TUSB4041I
Other Parts Discussed in Thread: TUSB4041PAPEVM, TPS74801
Hello,
I made a demo board for an 8-port HUB using 3 TUSB4041I. I used the design from the evaluation board TUSB4041PAPEVM but stripped out the EE-prom portion. I kept all the power control ICs and I followed the guidelines from the chip datasheet. After assembling the board, all the ports provide power when plugging a USB device to the port. However, there's no USB data connectivity. The main IC also doesn't show up in the device manager under Windows 7. The eval board shows up as a USB 2.0 MTT Hub. This suggests to me that the IC isn't interfacing to the computer via USB correctly.
I attached the schematic. Basically I use Master Hub to controller the 2 daughter hubs. I only use 2 USB lines from the Master Hub. On my board, all the USB lines are differential pairs when I route them. I tried to imitate the layout design on the eval board as much as I could. I'm not certain whether I'm missing something obvious to get this to work.
Thanks,
PatrickUSB_Hub_Demo.pdf