Part Number: TCAN1042H
Can you help me with this question from my customer:
"I am looking at TCAN1042 as part of the exercise to make sure the system power supply can handle bus fault current. From TCAN1042 datasheet, the published fault current is 180mA when CANH is biased at -12V. I wonder how this type of fault could occur in real applications. In addition, I wonder what the maximum transceiver current draw will be when either CAN_H or CAN_L is shorted to return or VCC?"