Part Number: DS90UB914A-Q1
We used 914/913 and found small percentage (<5%) of HW board has camera link issue:
- 914 LOCK pin toggle between 0 <->1, register 0x1C show parity error (bit[2]) and un-lock( bit[0]).
- 914 AEQ was enabled by default, register 0x4D read (0x20, bit[6] is 0). EQ value(register 0x4E) reads out value changes from 0x0 to 0xF. On good link, EQ value is stable, 0x0 or 0x1.
- Failed camera works fine on other HW boards; failed HW board works fine with other camera modules. Suspect there is some margin issue.