This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: RGMII mode strap options for DP83822I

Part Number: DP83822I

I need to configure my DP83822I in RGMII mode. Kindly provide the strap options that need to followed for the same. Do mention if the strap are for straight or cross connection.

Regards,

Nanda

  • RGMII is controlled thru Strap on pin RX_ER. You need to configure it to mode 2 or 3 depending whether AMDIX has to be enabled or disabled.

    RX_ER is PU on reset, please refer to table 9 for appropriate resistors to use. Please make sure the range for each mode is limited and high precision resistors ( 1%) shall be used.

    Regards,
    Geet