Part Number: TUSB4041I
Other Parts Discussed in Thread: TUSB4041PAPEVM,
The Switches explanation on pages 5-6 of the "TUSB4041PAP Evaluation Module" contradicts the "Pin Config" table, chapter 6.
Example:
Signal GANGED_HS_UP. The switch SW2.2 connects it to a Pullup.
the explanation of the switch goes as follows:
GANGED_HS_UP Switch. The TUSB4041 has an internal pullup on this terminal, so
ganged mode is enabled by default. If the switch is set to the ON position, the terminal is
pulled low and individual port power control mode is enabled. Since the
TUSB4041PAPEVM does implement individual port power controls, this terminal should
be set high.
Now the switch when ON will pull the pin HI, not LOW.
And the pin on the chip is described as "PD" so low by default.
There are several pins described like this, in opposite to the parts' datasheet. I am doing under-the-gun design and need a fast response with ALL THE SWITCH's PINS DESCRIPTION correct.