This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ethernet/USB/TTL to LVDS Serializer



Hello,

We have a customer with the following request, we are not having any luck tracking down a device with the following parameters:

"I have a transmitter that is operating at a fixed data rate of 100Mbps and takes LVDS (one channel and one clock) input. I am looking for a TTL/USB/Ethernet to LVDS serializer to connect to this transmitter. Ideally, I would like to send and receive datafile before connecting to the transmitter. Do you have a product or IC recommendation? I have looked into TSW1400EVM. I am not sure if it is the right one."

Could someone please advise?

Thanks,