This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822HF: About LED1 configuration on register and strap pin(mode).

Part Number: DP83822HF

Hello,

About LED1 configuration on register and strap pin(mode).

Regarding to LED1 configuration on DP83822HF, my customer is asking a question.
(Question)

・According to Table 14. LED_1 Configuration (page49),it is described as following.

(Strap mode 3&2 ): LED_1 configuration  LED_SPEED = 1  on for 100Mbps SPEED

・According to Table 14. LED_1 Configuration (page76),it is described as following.

(Register ): LED_1 control bit[11:8]= 0101 Speed, High for 100Base-TX

In case of each above configurations(register OR strap mode) , does LED1 become same behave on each condition?
(LED1 ON for 100Mbps SPEED)

Regards,
Tao 2199