This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925Q-Q1: Clarification of GPIO and GPO pins.

Part Number: DS90UB925Q-Q1

The data-sheet for DS90UB925Q-Q1 implies that GPIO[3:0] pins 36, 35, 26, 25 are capable of being outputs on the '925 serializer. Can you confirm that this is correct? Are they driven from data carried in the LS_BC or is my understanding incorrect?

The datasheet also implies that GPO_REG[8:6] (I2S_CLK / WC / DA) pins 13, 12, 11 are only capable of being outputs but the application note for enabling GPIOs implies that they are capable of also being inputs (page 3). Can you please confirm that this correct?

Application note from the DS90UB925Q-Q1 technical documents:

http://www.ti.com/lit/an/snla234/snla234.pdf