Hello support team,
I have a question about LMV221.
[Question]
How is the variation of the input level when output voltage is 1.5 V?
Frequency of the input signal is around 400 MHz.
Customer is using LMV221 now.
The customer is studying to design such that feedback is applied when the output voltage is 1.5V.
Best regads,
M. Tachibana