Part Number: TUSB546-DCI
Our project uses the Type-C for usb3.1 and DP functions, but in the debugging process we found that
DisplayPort AUX channel eye diagram failed when AUX snooping disable (pin CAD_SNK PU to VCC).
We use GPIO mode control,
So,
1.Please help to check which AUX snooping should be enable or disable when measure eye diagram?
2.The result of eye diagram is different between AUX snooping enable and disable, please check which is normal?
AUX snooping disable, result failed:
AUX snooping enable((pin CAD_SNK by internal PD )., passed:
3. The eye diagram on AUX snooping enable seems unexpected though eye diagram show passed, the waveform ramp down consistance...
Thanks!