This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DSI86: SN65DSI86 dual DSI input setting

Part Number: SN65DSI86

Dear Sir

I had a NB ODM customer want to use dual DSI input to drive 2140*1400 @ 60hz resolution.

My question is that do we have suggestion reg setting step to set the dual DSI register ? ( don't need the panel eDP output setting part )

I just want to compare with single DSI input register setting .

Please, thank you!

Best regards,

Bruce

  • Bruce,

    To enable the dual channel mode for SN65DSI86 the value in register 0x10 will need to be changed 1Eh from default value. Please refer to Table 21 and section 8.4.4.5 DSI Video Transmission Specifications for more information on dual channel mode for SN65DSI86.