This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB960-Q1: looking for compatible 14-16 bit cmos input serializer

Part Number: DS90UB960-Q1
Other Parts Discussed in Thread: DS90UB933-Q1, DS90UB913A-Q1

Hi,

I have a customer is inquiring about a 14-16bit (CMOS in) capable serializer that can work with the DS90UB960 deserializer.

I could only find up to 12bits, and found some RBG that can do higher number of bits.

They are also asking if it is possible to sample the signal at both clock edges.

Thank you,

Alberto

  • Hello-

    Unfortunately, there is no FPD-Link III serializer that is compatible with the DS90UB960-Q1 and that has more than 12 LVCMOS inputs. The compatible serializers with LVCMOS inputs (DS90UB913A-Q1 and DS90UB933-Q1) sample the signal at either rising (default) or falling edge, but not at both clock edges.

    Regards,
    Davor