Part Number: TUSB9260
Other Parts Discussed in Thread: TUSB9261
Tool/software: Linux
I used TUSB9260
and I tested TUSB9260 with HDD, SSD
SSD is work fine,
but, HDD is not working.
5V power supply is no problem,
but HDD is no spin up
Need some help.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Have you tried multiple HDD's -> Yes, I tried 2 type HDDs(SEAGATE, TOSHIBA) it's not working
but, WD(Western digital) HDD is working
And also working with 2 type SSD(SAMSUNG, Transend)
Also have you probed 5V to make sure that it does not dip on startup? -> Yes, I checked there's no voltage drop on startup
(when not working status, HDD is no spin up)