Hi Team,
Please advise me two questions bellow.
DS125DF410 will lock to the input which is compliant to 10G Ethernet,
CPRI etc. depending on the register 0X2F bit7:4] setting.
Among the standard setting, there is PROP3 its data rate is 6.25Gbps.
Q1. My question is that when the device is configured in this mode, how much
the data rate error can it tolerate, +/- 2000 ppm or more?
Q2. Can you let me know some more details of PROP3 standard?
Mita