Part Number: SN65LVDT388A
Hi,
In the IBIS model of the SN65LVDT388A device the termination resistors are missing. I'm aware of this post: e2e.ti.com/.../1460464
Because the simulation software extract the model out of the schematic I would like to include the termination resistors in the IBIS model rather than include the resistors in the schematic.
I would do the implementation of this resistors in the IBIS model as follows (showing the first input pin pairs):
[Series Pin Mapping] pin_2 model_name function_table_group
|
1 2 diff_term_110
3 4 diff_term_110
|
|************************************************************************
| 110 Ohm differential terminator
|************************************************************************
|
[Model] diff_term_110
Model_type Series
| (typ) (min) (max)
|
C_comp 0.0000pF 0.0000pF 0.0000pF
[Temperature Range] 25.0 85.0 -40.0
[Voltage Range] 3.3V 3.0V 3.6V
[R Series] 110 132 88
I'm unshure about the values of [Temperature Range], [Voltage Range] and [R Series].
Can a TI IBIS expert have a look on those values?
Thanks and best regards,
Patrick