This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB921-Q1: The YUV data format of 921 paired with 940

Part Number: DS90UB921-Q1

It is known from the specification that DS90UB921 can support YUV data. When 921 paired with 940,
If the input is YUV422, which 10 bits of 921 should be connected, D0 to D9, or D14 to D23? Thanks