This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65986: TPS6598x Customization Tool ver 3.16 - Can't Save File

Part Number: TPS65986

Ran into a problem using version 3.16 for the first time.  If I load our existing .pjt and try to save it to a new file (w/o changing anything), I get this error:

 

"Exception Encountered during Project File Save:sequence item 0: expected string, NoneType found

<type 'exceptions.TypeError'>"

 

The file is 0 bytes.  If I try to save over our existing .pjt, it just 0s the file out.

 

I notice the 'Transmit Source Capabilites' item is highlighted in red, but we just have the number of source PDOs set to 0. 

 

Any ideas?  I'll try to go back to a later version, but this is going to become a hot issue for us.  We need to use the new version's memory offset ability to generate a full binary image with our desired memory map for an upcoming factory build.