Part Number: TUSB4041I
Other Parts Discussed in Thread: TPS2001C
I am making the hub that should take the power from one of the devices and supply it to other devices and the OTG host (Raspberry Pi).
Only one of the devices is hot-pluggable (a memory stick), the rest are permanently plugged in inside the box and are not hot-plugged.
None has a battery.
I have used the TUSB4041I EVM board as the ref design.
So,
1. I think I should not be using the Power distributor (TPS2001 in my case) on all the device ports, considering one of them supplies the power.
2. Do I really want the Power Distributor on any device that is just a 5V USB device without battery and not hot-plugged?
3. I probably should use one on the external pluggable memory stick for short protection?
So I only need one of the TPS2001, not four?
Any advice?