This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About the LVDS output swing



I choose a device with 2.5V LVDS ouput ,and the output voltage swing is 250mV~450mV.

But the sink device is a 1.8V LVDS,and the input voltage require is 130mV~300mV.

How can I connect these two devices?