Part Number: TIC12400-Q1
Other Parts Discussed in Thread: TIC10024-Q1
Hi Team
I have some questions regarding ADC of TIC12400-Q1.
1. Are the TIC12400-Q1 and TIC10024 the same except for the ADC function?
2. Are the TIC12400-Q1and TIC0024-Q1 the same except for the parameters that are responsible for the ADC functions?
3. When monitoring the voltage input to the ADC input pin of the TIC12400-Q1 in real time, let me know the ADC error rate range.
4. Is hysteresis determined if ADC input pin is Active Low (Low detect)?
5. If hysteresis is defined, how much is the hysteresis range?
6. I know that the ADC input pin can set the threshold voltage. Can the user set the hysteresis region for the threshold voltage?
┌──────── Example of hysteresis in question 6 ──────┐
│ GND Switch Off detection threshold voltage = 5.0 V │
│ GND Switch On detection threshold voltage = 4.3 V │
└───────────────────────────────────┘
Can you set the hysteresis range of 0.7V as shown in the example above?
If so, please let me know how.
Thank you.