Part Number: DS90UB954-Q1
Other Parts Discussed in Thread: ALP
Hi team,
I have two questions.
#1
I would like to connect 953 and 954 originally in different hardware setting of clocking mode.
I will rewrite register of 953 through 954, but the back channel frequency is different depending on the initial value read by strap.
Does the back channel establish between SERDES different clocking mode?
#2
If 953 registers can be rewritten on back channel from 954, external clock input to CLKIN pin of 953.
Is it OK if the clock is externally input to 953 set to synchronous mode?
Best regards,
Tomoaki Yoshida