Part Number: TPS2553-1
Other Parts Discussed in Thread: TPS53353
Circuit diagram is very typical.
3.5V Vin, 1uF input capacitance, 100nF on the output, Fault pulled up to Vout by 100k, EN pin via 100k to the Vin.
The situation is following.
Current treshold is set to 100mA. 230K resistor from Pin ILim to GND. Now I connect 100 Ohm variable resistor to the output of TPS2553-1 and I slowly increase the load current. It should cut off the output when the overrcurrent is reached. But it does not. When I increase the load faster it switching off. But When I very slowly increasing the load by hand it is just limiting the current at 104mA, output voltage is reduced almost to 0, depend from the resistor setting, it can goes dow to 0 on full short. So it work but partially.
From my ubderstanding it should be switched off and latched after 8 ms of over-current. Or am I wrong?