Part Number: TPS2543
Hello,
i wanted to know how the IC regulates the current when a device tries to use more current than the previosly set limit.
The datasheet mentions that the IC regulates the Voltage down accordingly but not how.
Furthermore i planned on using the IC to charge a device without a Host on the other end of the data lines.
Is it still possible to put the device into the mode where it is only allowed to drain 500mA of current using the Datalines?
Thank you for the Help
best regards,
Tim