Part Number: TRS3253E
Hi.
I'm using the IC TRS3253E in a project and is appearing something about -9V in the pin "V-" (3) instead -5.5V.
This project consist in a CPU connected to TRS3253E.
All the charge pump capacitor are ok (100nF) and the power supply is 3,3V.
Some PCB's worked very well (appear -5-5V in pin "V-") but others have -9V in this pin "V-" (3).
I've verified that when I connect a 10K resistor from pin DIN2 (5) to GND these boards work very well (appear "-5,5V" in "V-"(3) ).
So I've imagined that the problem could be some reference... But I'm not sure.
Do you have any ideia what could be the reason of this problem?
Is this voltage (V-) created only by the charge pump capacitors? Or something can affect this value?
If the DIN pins don't have referente it could happens?
Thanks.