This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320HAI: GPIO mode

Guru 29720 points

Part Number: TUSB320HAI
Other Parts Discussed in Thread: TUSB320LAI, TUSB320

Hi Team,

My customer considers to use TUSB320HAI or TUSB320LAI for UFP application.

1)
Is there any criteria to decide GPIO mode or I2C mode?
I believe the difference is the following only and decision is up to customer.



2)
I believe OUT1 and OUT2 aren't required to be connected to MCU and can be left open if my customer uses GPIO mode.
Is my understanding correct?

Best Regards,
Yaita / Japan disty

  • 1. you can decide to use I2C mode or GPIO mode based on how you set the ADDR Pin. You can decide I2C mode or GPIO mode by if you want to read or write to the registers in the TUSB320 if you do not you can leave it in GPIO mode.

    2. They are not required to be connected to a MCU in GPIO mode.
  • Hi Michael-san,

    Thank you for your support.
    My customer considers to use TUSB320LAI with GPIO mode for UFP application however I asked the following in addition.

    1)
    My customer wants to know if it is possible to set only pull-down resistors(Rd) on CC pins without TUSB320LAI (CC controller) to achieve Type-C solution.
    Is it possible?
    I believe VBUS detection is also required but would like to have your comments.

    2)
    If my customer use the following solution, do you recommend VBUS OVP switch to protect VDD pin of TUSB320LAI from VBUS over voltage?
    He concerns VBUS overshoot when hot plug of Type-C cable.


    Best Regards,
    Yaita / Japan disty

  • it is possible to put pull down resistors on the CC lines but you will lose functionality like the ability to detect cable direction.

    The TUSB320 should not need any more OVP circuit but you can add it if you would like to.